Export Screen Shot 
 
                                        Export a screen shot from the DMM application.
By default, export operations are stored in the "Documents" folder on your computer and are organized by instrument type. 
For example – C:\Users\<user_name>\Documents\Keysight\PathWaveDMM\Exports\.
                                        For example – C:\Users\<user_name>\Documents\Keysight\PathWaveDMM\Exports\.
You can export a screen shot of the current view to the Windows clipboard, an image file (PNG, JPEG, or BMP format), or a Microsoft Word file.
- Click here to see an example of a screen shot exported from the Screen Image view as a BMP (bitmap) file.
 - Click here to see an example of a screen shot of a chart exported from the Data Logger view or Digitizer view as a JPEG graphics file (you can also export in PNG or BMP format).
 
Below are the Export File dialog details:
Export File Details
File Name
- From the Instrument View, the default file name is "Instrument View Screen Capture". To change the default name, click on the existing name and edit it.
 - From the Screen Image view, the default file name has a "ScreenImage" prefix followed by a numeric index. For example, ScreenImage 0. To change the default name, click on the existing name and edit it.
 - From the Data Logger view, the default file name is "Datalog Screen Capture". To change the default name, click on the existing name and edit it.
 - From the Digitizer view, the default file name is "Digitizer Screen Capture". To change the default name, click on the existing name and edit it.
 Export Path - From the Screen Image view only, the currently selected path for saving the file on your computer. To change the path, click Browse... and browse to a different path.
File Type - From the Screen Image view only, select the desired export file format. Select from image (PNG, JPEG, or BMP format) file or Microsoft Word (.docx) file.